Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
I2C and SMBus Solutions Slide 11

Some of the most common applications for the TCA6408A and TCA6416A are housekeeping functions, such as temperature and humidity sensors, and status indicators of LEDs, as well as hardware control monitors. This is visually illustrated in the diagram on the slide. Please note that the red lines are input devices and the blue lines are outputs. This shows how the devices can simultaneously interface between input and output devices.

PTM פורסם ב: