Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
I2C and SMBus Solutions Slide 3

As was mentioned earlier, I²C devices can be used in a wide range of applications. Shown in this slide is a block diagram highlighting I²C usage in the server segment. In this generic server application, there are two areas where I²C devices can be used. The first is in conjunction with the BMC, or base-board management controller, performing housekeeping duties such as fan control and humidity control. The next application is card detect signals for the hot plug controllers. I²C devices can be used in other areas too, however to keep things simple, only two areas are highlighted in this example.

PTM פורסם ב: