Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Porting Projects from StellarisWare to TivaWare for C Series Slide 2

TivaWare for C Series is an extensive suite of software designed to simplify and speed up embedded application development using Tiva C Series MCUs. TivaWare for C Series includes powerful Peripheral Driver Library, Graphics Library, USB Library, and Sensor Library which have several APIs to configure and initialize different peripherals of the Tiva C Series MCUs. The libraries come with the source code which is pre compiled for use 'as-is' or can be adapted as desired. TivaWare for C Series also includes boot loader, several code examples, and third party packages that provide a very comfortable starting point. It also allows the customer to focus on application development and not so much on how to set up the MCU.

PTM פורסם ב: