Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Porting Projects from StellarisWare to TivaWare for C Series Slide 5

Texas Instruments goal is to provide a unified experience to the customer with different products from the Tiva family of products. Because of this, some cosmetic changes have to be made, such as the directory paths. Now, the customer can locate all TI software such as TivaWare for C Series, Code Composer Studio, uniFlash, and Pin Mux utility in one directory. An example of this is C:/ti for a cleaner and more organized look. Due to user confusion over the location of code examples, board-specific example applications have now been moved into the examples directory under the board subdirectory. Now the customer can find board specific and peripheral specific examples in the same directory. Examples within TivaWare reference the local directory, but if the customer has already developed software outside of the StellarisWare directory, the developer will have to change the paths for the files that are referenced in the project.

PTM פורסם ב: