Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
The Ultra Low Power MSP430 Slide 17

Here the possibilities of clocking the MSP430 with the basic clock are shown. The MSP430 can be run without a crystal because the DCO, the on-chip oscillator, functions completely independently from the crystal oscillator. The lower left shows the most common application of using the 32768 crystal for the low power A Clock signal. The DCO can also be sourced through an external resistor called ROSC. In this case, the external resistor allows a current to be injected into the DCO, controlling its frequency and reducing its temperature drift.

PTM פורסם ב: