Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
The Ultra Low Power MSP430 Slide 19

As just mentioned, the DCO has a modulator that mixes two adjacent DCO frequencies. Looking at the DCO clock on an oscilloscope, there will be a clock signal that contains two discrete frequencies. The mixing of the two frequencies provides a couple of benefits: 1) It allows a finer control over the effective frequency that the DCO clock provides and 2) It provides for a lower EMI device. The MSP430 has very low EMI emissions due to the mixing of the two frequencies.

PTM פורסם ב: