Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Tiva C Series TM4C123x USB Slide 12

Communications Device Class (CDC) is generally implemented in embedded systems like mobile phones to achieve more than one functionality from the device, so that a phone may be used as a modem, fax, or network port. This class provides simple serial communication functionality. Refer to the USB CDC Serial example in TivaWareTM for C Series as a starting point for more complex serial communications and file transfers. The data interfaces are generally used to perform bulk data transfer using Bulk USB Device. There is an example program in TivaWare that features a simple data-echoing application. This serves as a basis for a more complicated data transferring application.

PTM פורסם ב: