Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Tiva C Series TM4C123x USB Slide 7

TivaWare for C Series is an extensive suite of software designed to simplify and speed up embedded application development using Tiva C Series MCUs. This software includes the Peripheral Driver Library, Graphics Library, USB Library, and Sensor Library, which include several APIs to configure and initialize different peripherals of the Tiva C Series MCUs. These libraries come with the source code which is mostly in C. They are pre-compiled for use 'as-is' and can also be adapted as desired. TivaWare for C Series also includes a boot loader, several code examples, and third party packages that allow the user to focus on their application development and not so much on how to set up the MCU.

PTM פורסם ב: