Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
MSP430FR5969 LaunchPad Part 6 Slide 2

The source code for the lab, as well as this power point presentation is available from the link shown on this slide. An easy way to find it is to go to the processors.wiki.ti.com site and then search for the term FR59xx Training Workshop. On the wiki page, browse to the LaunchPad section and then download the lab zip file from the link marked “lab material”. On opening the zip file, copy and paste the folder LAB2a ADC12B into a workspace directory. Now the project for the lab is set up.

PTM פורסם ב: