Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
MSP430FR5969 LaunchPad Part 6 Slide 5

To begin the lab, open the source code LAB 2A ADC12B.c in the project folder. Use the comments as a guide and setup the ADC using DriverLib as explained in training module 4. Once the lab exercise is complete, test the code by tying the ADC input channel to VCC or Ground to check whether the LED turns on or stays off.

PTM פורסם ב: