Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Power Factor Correction Slide 5

This circuit shows a common continuous conduction mode power factor correction scheme for higher power levels. Two PFC stages are placed in parallel to deliver higher power and is better from a thermal management perspective as the power handling is spread over two stages over a wider area of the PCB. In a parallel configuration, the higher input and output ripple currents are the result of the addition of the two stages as expected.

PTM פורסם ב: