Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Power Factor Correction Slide 6

In the interleaved circuit, the two stages are set 180° out of phase to each other. Therefore, the addition of two phases 180o out of phase causes the ripple current to cancel when added. Notice that the ripple current has been significantly reduced from the parallel method. Ripple current cancellation can save significant systems cost as the EMI filter and the output capacitor/s don’t need to attenuate typically high ripple current.

PTM פורסם ב: