Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Powering FPGAs with SIMPLE SWITCHER LMZ3 Power Modules Slide 5

Many FPGAs  have sequencing requirements in order to power an FPGA. Sequencing requirements can limit the inrush current during the power up stage of the FPGA. For FPGAs that do not have sequencing requirements, devices such as microcontrollers may have such requirements. Ignoring sequencing can damage devices which will cause devices to malfunction. A simple way to implement power up sequencing is to use voltage regulators with inhibit feature, such as the LMZ3 power modules. Other options for sequencing would be to use sequencer devices such as the LP3470 and supply voltage supervisors such as the LM3880.

PTM פורסם ב: