Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
XC9235-9236 Slide 9

The 3MHz version has an even lower ripple voltage performance than the 1.2MHz version shown on the previous slide. The XC9236A18DMR-G 3MHz device has a low 7mV ripple voltage. The Torex PFM/PWM auto shifting control scheme is one large advantage which Torex has over its competitors.

PTM פורסם ב: