Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
ex

For example, when measuring 10 A through the CT’s primary, it will develop a current on the secondary that is directly proportional to the turns ratio of the transformer. The voltage across the burden resistor connected to the secondary of the transformer will develop a voltage that is also proportional to the current by Ohm's Law.

PTM פורסם ב: