Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
IntegratedConnector-Slide11

In order to meet electrical standards, the components within the ICM must provide isolation which is done with isolation transformers, and EMI suppressionthat is done with the common mode chokes. Termination of the unused pairs, within certain communication standards, is accomplished with what is known as a Bob Smith termination, which is composed of 75 ohm resistors and a 1000 pF, 2000V capacitor.

PTM פורסם ב: