Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Opto IGBT and MOSFET Driver Slide 13

Having a low input supply current is a clear benefit to customers. It reduces power consumption, resulting in less heat generation. With less heat, less heat dissipation is required allowing the use of smaller heat sinks. As the operating temperature increases, the supply current decreases. Note that at 25°C and higher, the input current will be less than 1.5 mA.

PTM פורסם ב: