Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Opto IGBT and MOSFET Driver Slide 2

To best explain what an IGBT driver does, reference will be made to the industrial application illustrated here; the control of a 600 V, 3-phase motor moving a robotic arm. The low voltage sensitive electronics and user interface are shown on the left while the high voltage and potentially noisy motors are on the right. Notice that there is a feedback loop from the robotic arm to the controller providing speed, position and status data.

PTM פורסם ב: