Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
TrenchFET Gen IV MOSFETs PowerPAIR Slide 10

Beyond the standard MOSFET, TrenchFET Gen IV also enables an application specific version, the SKYFET. Vishay’s SKYFET devices feature a monolithic Schottky diode which exhibits soft reverse recovery. The result is higher efficiency across the load compared to devices without Schottky. The graph on left side of this slide illustrates the efficiency improvement of SKYFET by comparing two devices with identical high-side MOSFET in the same PowerPAIR packaging. Even though SiZ914DT has higher Rds(on), the improvement of using SKYFET was a worthwhile trade-off.

PTM פורסם ב: