Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
TrenchFET Gen IV MOSFETs PowerPAIR Slide 7

The switching applications for TrenchFET Gen IV include single-phase or multi-phase synchronous buck converters, and secondary side synchronous rectification in isolated DC-DC topologies. The low Rds(on) characteristic is also ideal for high current static switch applications such as OR’ing in power redundancy, hot-swap switch, and high current load switch. These devices will also provide very low loss for DC motor drive.

PTM פורסם ב: