Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
HVArc Guard Surface Mount MLCC Slide 2

Ceramic chip capacitor surface arc-over can occur when a high enough voltage is applied across the capacitor to create an electrical arc across its surface which can cause an electromagnetic field break down of the dielectric material creating a short circuit condition. One way to inhibit surface arc-over would be to keep the surfaces of the capacitor free of conductive foreign material that could create a path of least resistance between the terminations.

PTM פורסם ב: