Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
General Purpose DC-DC Converters Slide 3

To help with the selection of the ideal DC/DC converter for the project, the engineer will need to determine a few critical parameters: input voltage, input voltage range, output voltage and current draw. Additionally, the engineer will have to consider how much actual space is available on the PCB.

PTM פורסם ב: