Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Würth-Slide4

On this slide, users can see a typical layout of a SEPIC converter from Linear Technology which uses two 22µH inductors, or L1 and L2, in the circuit. The capacitor, C6, basically splits the windings in a primary and a secondary. This design can now be done like shown in this example by using two individual inductors with 22µH, but there are clear advantages when using one of Würth Elektronik coupled inductors in this design. The construction and the advantages of a coupled inductor will be shown on the next slides.

PTM פורסם ב: