Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Test Setup

When testing the 24 V to 15 V WE-PPTI 1308 part, the closest competitor part was chosen to test alongside. The Würth Elektronik part has 18% less volume than the competitor part while having a significantly lower profile as well. Both parts were tested on the SN6507 EVM available from Texas Instruments with no component changes for the default 1 MHz operation. Both parts were also tested at 400 kHz.

PTM פורסם ב:
PTM Updated on: 2024-04-29