Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Set Switching Frequency on SN6507

In order to test the board with the transformers at 400 kHz, a clock resistor must be added to the evaluation module. With no added resistor, the EVM will run at 1 MHz. Using the chart in the SN6507 datasheet, the clock resistor was determined to be 30 kΩ and was added to the EVM when testing at 400 kHz.

PTM פורסם ב:
PTM Updated on: 2024-04-29