Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
ECP180 Series Slide 8

Here the expanded scale shows more details. Maximum efficiency occurs at the maximum convection rating, the most critical operational point to minimize waste heat. Once airflow is introduced, it is still important to minimize waste heat in order to minimize airflow requirements. This level of efficiency is market leading with the lowest efficiency 12 V model maintaining in excess of 91% convection cooled at the lowest line input. Head-line efficiency is 95% at high line input.

PTM פורסם ב: