Maker.io main logo

Making REAL Fallout Power Armor (Part 3)

825

2024-12-20 | By The Hacksmith

Our adventure to build our community's most requested - Fallout's Power Armor - continues!

In the Fallout universe, Power Armor is a wearable exoskeleton that augments the wearer's strength, endurance, and resilience, protecting them from the unforgiving nuclear wasteland and its belligerent residents. It lets you run faster, go further, carry more, and survive everything from radroach bites to gunshots.

In episodes one and two, we built the structure for the upper body of the armor, leaving a super powerful exoskeleton torso ready for business. If you haven't seen those episodes, you can watch them here:

In this installment, we tackled the next challenge: a fully functional helmet with Heads up Display and packed full of useful gadgets for keeping you alive at nighttime in a nuclear wasteland. Here’s what we are going for:

  • Heads Up Display (HUD) using modified Rayneo augmented reality glasses.
  • Thermal vision using an InfiRay thermal camera.
  • Night vision using a Raspberry Pi camera with no IR filter.
  • Zoom vision using a Raspberry Pi camera with an adjustable zoom lens.
  • Mining light and IR light (for night vision) with a custom lighting PCB from JLCPCB
  • Respirator connected to a second stage regulator to run on tank air and a switch to run off a filter instead.
  • Geiger counter using a Radiacode Bluetooth Geiger counter.
  • Actuated faceplate, mask, and cameras using pneumatic cylinders running on the power pack pressure tank.
  • I2C Heart rate monitor (MAX30101)
  • I2C Arduino Compass (Grove 10DOF IMU)

Image of REAL Fallout Power Armor

So how are we going to make this? Well like most things at Hacksmith, it starts with a 3D model in Solidworks. Luckily, we have a great starting point from our friends at Thangs. The trick is to then find a place inside the helmet for all of the components to fit. With the design complete, we 3D printed everything, cleaned it up, and gave it a quick paint job. For bonus points, we added a set of actuators to move the visor of the helmet up and away from the wearer as seen in the game. Testing found that this motion interfered with the camera and lighting boom sticking out from the right ear of the helmet, so a second set of actuators was needed to swing the boom out of the way of the moving visor. This used the last two valves that were provided back in the first episode. Later on, we are going to Nanovate the entire suit to make it bulletproof but for now, the paint looks pretty good.

With the helmet built, it was time to add in all the electronics. Everything feeds into the Nvidia Jetson Xavier NX which acts as the brain of the helmet. The Jetson then adds an overlay graphic that is displayed on the augmented reality glasses. This shows the wearer basic operating stats of the suit, as well as their own vital signs. We are using sensors like a MAX30101 heart rate sensor and pulse oximeter mounted in the user interface, a battery voltage monitor ADC, a pressure transducer reading out the pressure of the compressed air reservoir, a nine-axis IMU which is processed to provide a compass heading - a critical navigation tool! - and an ionizing radiation sensor to detect the true unseen hazard of a nuclear wasteland, the nuclear waste.

Integrating all of this was quite the adventure, and if you want to see how we put it all together, check out the full schematic here:

Image of Fallout Power Armour Scheme-it

Download Schematic

To aid with nighttime navigation or combat, an array of cameras can be superimposed on the HUD. There is an optical zoom camera, a thermal camera, and an infrared night-vision camera. An infrared and a visible light illuminator are provided, built into the camera boom arm on the helmet. These provide extremely bright lighting for the cameras - so bright that the infrared light needs a small warning LED to be included to avoid eye damage to onlookers from the intense infrared radiation! These two lights can be switched on or off according to the needs of the user.

Of course, to build any of this, we need a robust model of the armor as a whole, and ours is available for download via Thangs - fully 3D printable for cosplay!

In the grand finale of the video, Bogdan tested out the entire system by going on a little scavenger hunt to find a radioactive relic of the wasteland.

This project is only getting started, so subscribe and tune in next time to see the Fallout Power Armor really take shape!

מק"ט יצרן # SC1223
RASPBERRY PI CAMERA 3
Raspberry Pi
מק"ט יצרן # 1280
SMT TEST SOCKET - TSSOP-28 BREAK
Adafruit Industries LLC
מק"ט יצרן # 2903361
RELAY GEN PURPOSE SPST 6A 24V
Phoenix Contact
מק"ט יצרן # MEC0251V3-000U-A99
FAN AXIAL 120X25MM 12VDC WIRE
Sunon Fans
מק"ט יצרן # PIM438
MAX30101 BD HEART SMOKE OXIMETER
Pimoroni Ltd
מק"ט יצרן # CF1/4CT52R103J
RES 10K OHM 5% 1/4W AXIAL
KOA Speer Electronics, Inc.
מק"ט יצרן # SIR19-21C/TR8
EMITTER IR 875NM 65MA 0603
Everlight Electronics Co Ltd
מק"ט יצרן # JB2835BWT-G-H40GA0000-N0000001
LED J NEUTRAL WHT 4000K 1411
Cree LED
מק"ט יצרן # CMD17-21VRD/TR8
LED RED DIFFUSED 0805 SMD
Visual Communications Company - VCC
מק"ט יצרן # CAM009
160 (FISHEYE) NIGHT VISION CAMER
Pimoroni Ltd
מק"ט יצרן # CMF5510K000BEEB
RES 10K OHM 1/2W 0.1% AXIAL
Vishay Dale
מק"ט יצרן # 101020252
GROVE - IMU 10DOF V2.0
Seeed Technology Co., Ltd
מק"ט יצרן # PURETHERMAL-3-FS1
PURETHERMAL 3 WITH LEPTON FS
GroupGets LLC
מק"ט יצרן # YR1B14KCC
RES 14K OHM 0.1% 1/4W AXIAL
TE Connectivity Passive Product
מק"ט יצרן # MIPAN2XX500PAAAX
MIP, RAT., 500PSIA, PACKARD, N2
Honeywell Sensing and Productivity Solutions
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.