Maker.io main logo

CircuitPython CLUE I Ching Caster

41

2024-07-26 | By Adafruit Industries

License: See Original Project Displays LCD / TFT

Courtesy of Adafruit

Guide by Carter Nelson

Overview

circuitpython_output

In this guide we will show you how you can use your Adafruit ‎CLUE to consult the ancient Chinese text known as the I Ching, or ‎Book Of Change. With a simple shake of your CLUE board, you can ‎tap into the mystic forces of the universe and come up with a ‎‎"random" hexagram that forms the basis of a reading used to ‎consult the I Ching.‎

So, grab a CLUE, load the code, balance your chi, and have some fun! ‎

Ommmmmmm.‎

Adafruit CLUE - nRF52840 Express with Bluetooth LE

clue_1

I Ching Summary

text_2

The I Ching is an ancient text. As such, there are numerous ‎descriptions of what it is and what it has become. To keep things fun ‎and simple, we are going to use a very brief description here.‎

The I Ching is comprised of 64 separate entries. Each entry is ‎associated with a hexagram along with a collection of text that reads ‎like poetry. Let's cover a few details.‎

Yin and Yang

The most fundamental basis for the I Ching is the concept of Yin and ‎Yang - the two intertwined forces that drive the universe. Can't have ‎one without the other. Light and dark. Sweet and sour. Etc.‎

A common way to represent Yin and Yang is with line segments like ‎this:‎

yinyang_3

These two lines are put together to create further symbols called ‎trigrams, a stack of 3, and hexagrams, a stack of 6.‎

Trigrams and Hexagrams

The two lines representing Yin and Yang are put together in groups ‎of 3 to comprise 8 trigrams which are considered to comprise the ‎basic elements, like "Earth" and "Mountain". The trigrams are then ‎stacked in groups of two to create the 64 unique hexagrams.‎

The basis here is essentially binary, 0=Yin and 1=Yang. The prefix "tri" ‎means 3 and "hex" means 6. So, the hexagrams are like a 6 bit value ‎‎(2^6 = 64). They are read from bottom to top, so you end up with ‎something like this:‎

yinyang_4

This binary interpretation is not really used in the I Ching. But it is ‎useful for our code. We don't need any fancy storage mechanism to ‎correlate a specific hexagram with a given number from 0 to 63 (64 ‎total). We can simply use the binary representation of that number ‎to generate the hexagram. For example, let's say we somehow came ‎up with 42 as our "reading". Then we can do something like:‎

Download File

Copy Code
>>> print("0b{:06b}".format(42))
0b101010
>>>

and use each of the bits to generate a corresponding line for the ‎hexagram. Each 0 becomes a dashed line Yin and each 1 becomes a ‎solid line Yang.‎

Consulting the I Ching

For each of the 64 hexagrams there is an entry in the I Ching with a ‎bunch of vague poetics like text. These 64 entries comprise the I ‎Ching - it's basically a reference text.‎

Since the I Ching itself is nothing but a collection of 64 entries, how is ‎it used? To "consult" the I Ching you must come up with a number ‎from 1 to 64. And then you look up the I Ching entry for that ‎hexagram number. While this process should be something ‎intrinsically random, the idea is that you should be involved in this ‎randomness and thus give a "reading" that is unique to you. This is ‎referred to a cleromancy.‎

There are approaches that involve shaking a bundle of sticks, ‎flipping coins, etc. But once you have the value, you then just look it ‎up in the I Ching.‎

I Ching Hexagram Table

Of course, making sense of what the actual words are trying to tell ‎you is another story. Seek out an old mystic living in a cave on a ‎mountain for help.‎

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY flash drive to iterate.‎

The following instructions will show you how to install CircuitPython. ‎If you've already installed CircuitPython but are looking to update it ‎or reinstall it, the same steps work for that as well!‎

Set up CircuitPython Quick Start!‎

Follow this quick step-by-step for super-fast Python power :)‎

Download the latest version of CircuitPython for CLUE from ‎circuitpython.org

Click the link above to download the latest version of ‎CircuitPython for the CLUE.‎

Download and save it to your desktop (or wherever is handy).‎

click_5

Plug your CLUE into your computer using a known-good USB cable.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! So, make sure you have a USB cable you know is good ‎for data sync.‎

Double-click the Reset button on the top (magenta arrow) on your ‎board, and you will see the NeoPixel RGB LED (green arrow) turn ‎green. If it turns red, check the USB cable, try another USB port, ‎etc. Note: The little red LED next to the USB connector will pulse red. ‎That's ok!‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

board_6

You will see a new disk drive appear called CLUEBOOT.‎

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.‎

disk_7

disk_8

The LED will flash. Then, the CLUEBOOT drive will disappear, and a ‎new disk drive called CIRCUITPY will appear.‎

If this is the first time, you're installing CircuitPython or you're doing ‎a completely fresh install after erasing the filesystem, you will have ‎two files - boot_out.txt, and code.py, and one folder - lib on ‎your CIRCUITPY drive.‎

If CircuitPython was already installed, the files present before ‎reloading CircuitPython should still be present on ‎your CIRCUITPY drive. Loading CircuitPython will not create new ‎files if there was already a CircuitPython filesystem present.‎

That's it, you're done! :)

newdisk_9

Code

The code for the CLUE I Ching Caster is listed below. You can copy it ‎out and save it to a local file. Once you've done that, you can save ‎the file as code.py in your CIRCUITPY folder and it will run ‎automatically when powered up or reset. You'll also need to grab the ‎font file christopher_done_24.bdf.‎

christopher_done_24.bdf

You CIRCUITPY folder should look something like this:‎

folder_10

Libraries

You'll need to make sure the following libraries are installed in ‎your CIRCUITPY/lib folder:‎

  • adafruit_apds9960‎
  • adafruit_bitmap_font
  • adafruit_bus_device
  • adafruit_display_text
  • adafruit_register
  • adafruit_bmp280.mpy
  • adafruit_clue.mpy
  • adafruit_lis3mdl.mpy
  • adafruit_lsm6ds.mpy
  • adafruit_sht31d.mpy
  • neopixel.mpy

You can find more info on downloading and installing libraries here:‎

CircuitPython Libraries

When you're done, your CIRCUITPY/lib folder should look like this:‎

libraries_11

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 Carter Nelson for Adafruit Industries
#
# SPDX-License-Identifier: MIT

import time
import random
import displayio
from adafruit_bitmap_font import bitmap_font
from adafruit_display_text import label
from adafruit_clue import clue

#--| User Config |-------------------------------
BACKGROUND_COLOR = 0xCFBC17
HEXAGRAM_COLOR = 0xBB0000
FONT_COLOR = 0x005500
SHAKE_THRESHOLD = 20
MELODY = ( (1000, 0.1), # (freq, duration)
(1200, 0.1),
(1400, 0.1),
(1600, 0.2))
#--| User Config |-------------------------------

# Defined in order treating each hexagram as a 6 bit value.
HEXAGRAMS = (
"EARTH", "RETURN", "THE ARMY", "PREVAILING", "MODESTY", " CRYING\nPHEASANT",
"ASCENDANCE", "PEACE", "WEARINESS", "THUNDER", "LETTING\n LOOSE",
"MARRYING\n MAIDEN", " SMALL\nEXCESS", "ABUNDANCE", "STEADFASTNESS",
" GREAT\nINJURY", "SUPPORT", "RETRENCHMENT", "WATER", "FRUGALITY",
"ADMONISHMENT", "FULFILLMENT", "THE WELL", "WAITING", "ILLNESS",
"THE CHASE", "TRAPPED", "LAKE", "CUTTING", "REVOLUTION", " GREAT\nEXCESS",
"STRIDE", "LOSS", "THE CHEEKS", "BLINDNESS", "DECREASE", "MOUNTAIN",
"DECORATION", "WORK", " BIG\nCATTLE", "ADVANCE", "BITING", "UNFULFILLMENT",
"ABANDONED", "TRAVELER", "FIRE", " THE\nCAULDRON", " GREAT\nHARVEST",
"VIEW", "INCREASE", "FLOWING", "SINCERITY", "PROGRESS", "FAMILY", "WIND",
" SMALL\nCATTLE", "OBSTRUCTION", "PROPRIETY", "THE COURT", "TREADING",
"LITTLE\n PIG", "GATHERING", "RENDEZVOUS", "HEAVEN",
)

# Grab the CLUE's display
display = clue.display

# Background fill
bg_bitmap = displayio.Bitmap(display.width, display.height, 1)
bg_palette = displayio.Palette(1)
bg_palette[0] = BACKGROUND_COLOR
background = displayio.TileGrid(bg_bitmap, pixel_shader=bg_palette)

# Hexagram setup
sprite_sheet = displayio.Bitmap(11, 4, 2)
palette = displayio.Palette(2)
palette.make_transparent(0)
palette[0] = 0x000000
palette[1] = HEXAGRAM_COLOR

for x in range(11):
sprite_sheet[x, 0] = 1 # - - 0 YIN
sprite_sheet[x, 1] = 0
sprite_sheet[x, 2] = 1 # --- 1 YANG
sprite_sheet[x, 3] = 0
sprite_sheet[5, 0] = 0

tile_grid = displayio.TileGrid(sprite_sheet, pixel_shader=palette,
width = 1,
height = 6,
tile_width = 11,
tile_height = 2)

hexagram = displayio.Group(x=60, y=15, scale=10)
hexagram.append(tile_grid)

# Hexagram name label
# font credit: https://www.instagram.com/cove703/
font = bitmap_font.load_font("/christopher_done_24.bdf")
font.load_glyphs(b'ABCDEFGHIJKLMNOPQRSTUVWXYZ')
hexname = label.Label(font, text=" "*40, color=FONT_COLOR)
# this will initially hold the "shake for reading" message
hexname.text = " SHAKE\n FOR\nREADING"
hexname.anchor_point = (0.5, 0.5)
hexname.anchored_position = (120, 120)

# Set up main display group (splash)
splash = displayio.Group()
display.root_group = splash

# Add background and text label
splash.append(background)
splash.append(hexname)

def show_hexagram(number):
for i in range(6):
tile_grid[5-i] = (number >> i) & 0x01

def show_name(number):
hexname.text = HEXAGRAMS[number]
hexname.anchored_position = (120, 180)

#===================================
# MAIN CODE
#===================================
print("shake")
# wait for shake
while not clue.shake(shake_threshold=SHAKE_THRESHOLD):
pass

# calibrate the mystic universe
x, y, z = clue.acceleration
random.seed(int(time.monotonic() + abs(x) + abs(y) + abs(z)))

# cast a reading
reading = random.randrange(64)
print("reading = ", reading, HEXAGRAMS[reading])

# play a melody
for note, duration in MELODY:
clue.play_tone(note, duration)

# prompt to show
display.auto_refresh = False
hexname.text = " GOT IT\n\nPRESS BUTTON\n TO SEE"
hexname.anchored_position = (120, 120)
display.auto_refresh = True
while not clue.button_a and not clue.button_b:
pass

# and then show it
display.auto_refresh = False
splash.append(hexagram)
show_hexagram(reading)
show_name(reading)
display.auto_refresh = True

# hold here until reset
while True:
pass

View on GitHub

Usage

Here's how to use.‎

  • Save the program as code.py
  • Press RESET
  • Should see screen that say "SHAKE FOR READING"‎

save_12

  • You should hear a little melody play
  • The screen will change to "PRESS BUTTON TO SEE"‎

press_13

  • Once you press either A or B button, you should see your ‎hexagram
  • If you want to try again, press RESET to start over

reset_14

Customizing

There are various settings you can change at the top of the code. ‎Look for these lines:‎

Download File

Copy Code
#--| User Config |-------------------------------
BACKGROUND_COLOR = 0xCFBC17
HEXAGRAM_COLOR = 0xBB0000
FONT_COLOR = 0x005500
SHAKE_THRESHOLD = 20
MELODY = ( (1000, 0.1), # (freq, duration)
(1200, 0.1),
(1400, 0.1),
(1600, 0.2))
#--| User Config |-------------------------------

You can change the colors, the shake threshold, as well as the little ‎melody that plays.‎

A Note on Translation

The original text of the I Ching was written in ancient Chinese. The ‎translation into English used here is based on the text by Kerson and ‎Rosemary Huang (ISBN 978-0894803192).‎

Drawing the Hexagram

Let's go into some detail about the approach taken to draw the ‎hexagram. This is a handy little trick that maybe you can reuse in ‎one of your projects. It uses a very simple and tiny sprite ‎sheet Bitmap to source the two basic line symbols used to generate ‎the hexagram. These are then used in a TileGrid to generate the ‎actual hexagram. To render this large on the display, the ‎displayio Group's scale feature is used.‎

Sprite Sheet

For a more in-depth overview of what a sprite sheet is, see this ‎section of the displayio guide:‎

Sprite Sheet

Look again at the two lines that comprise the hexagram. They are ‎very basic - just a line and dashed line. We can represent these with ‎a simple bitmap like this:‎

spritesheet_15

This bitmap is only 11 pixels wide by 4 pixels high. Each blue square ‎is a pixel. The two blank lines are there for padding. The width was ‎chosen for basic aesthetic reasons, generating a nice overall aspect ‎ratio for the lines. This bitmap is so simple that it is generated ‎programmatically. That's what these lines of code are doing:‎

Download File

Copy Code
for x in range(11):
sprite_sheet[x, 0] = 1 # - - 0 YIN
sprite_sheet[x, 1] = 0
sprite_sheet[x, 2] = 1 # --- 1 YANG
sprite_sheet[x, 3] = 0
sprite_sheet[5, 0] = 0

Using a Tile Grid for the Hexagram

The sprite sheet can then be used along with a TileGrid to generate ‎any of the 64 hexagrams. The TileGrid will be 1 column by 6 rows - ‎one row for each line of the hexagram. Each cell is 11 pixels wide by 2 ‎pixels high, corresponding to one of the symbols from the sprite ‎sheet.‎

Then it's a simple matter of setting the source index for each cell of ‎the TileGrid to point to one of the two available bitmaps from the ‎sprite sheet. For example, to make the 3rd line down a dashed (Yin) ‎symbol, we would do something like this:‎

index_16

To generate the entire hexagram, we just set each cell in the TileGrid ‎to a source from the sprite sheet. Like this:‎

generate_17

Some thought has been put into the arrangement of the sprite sheet. ‎By making the dashed (Yin) symbol be first, we can then generate a ‎hexagram from any integer 0 to 63 (64 total) by simply using each of ‎its bits to set the TileGrid's sources.‎

In the example above, that would be 0b100101 = 37. Remember, the ‎least significant bit is on the bottom.‎

That general approach is what is being down in ‎the show_hexagram function:‎

Download File

Copy Code
def show_hexagram(number):
for i in range(6):
tile_grid[5-i] = (number >> i) & 0x01

Using Scale to Embiggen

In its raw form, the sprite sheet is only 11 pixels wide by 4 pixels high. ‎The hexgram created from the sprite sheet ends up being 11 pixels ‎wide by 12 pixels high. That's pretty small. So how can we make it ‎bigger on the display? By using scale.‎

The scale parameter is an option for the displayio.Group class. It is ‎used as a multiplier when rendering the contents of the Group. Every ‎pixel is drawn "scale" number of times. So, if scale=3, then every 1 ‎pixel would become 3x3 pixels on the display.‎

A scale factor of 10 is used for the hexagram, which is specified in ‎this line of code:‎

Download File

Copy Code
hexagram = displayio.Group(max_size=1, x=60, y=15, scale=10)

So, the 11x12 hexagram ends up being drawn at an actual size of ‎‎110x120 pixels.‎

There's no fancy smoothing done, which can lead to a very coarse ‎look to the scaled-up bitmap. However, since our shapes are blocky ‎rectangles, this works out just fine.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.