Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Phase-Slide3

This picture illustrates the internal structure of a BGA type component. For a high powered device the majority of heat is dissipated through the case of the component and into the heatsink. The resistance from the component to the heatsink must be understood as it is critical to the device temperature.

PTM פורסם ב: