Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Phase-Slide4

There are several types of interface materials, which cover a wide range of applications. There are TIMs that provide mechanical attachment, such as tape and epoxy, and other types of TIM such as phase change and grease need to be secured with a mechanical attachment method. Gap filler material is used when large distances need to be coupled and are not usually used for cooling high powered devices.

PTM פורסם ב: