Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Specialty Sensor Assemblies

Amphenol Advanced Sensors offers a full line of specialty sensor assemblies that are ideal for appliance applications. There is a clip-on pipe sensor which is an NTC thermistor assembly fitted with spring metal clips that allow the sensor assembly to clip directly to the pipe surface. The inline flow-through sensor is an NTC thermistor assembly designed to allow fluid to pass directly through the assembly. The self-adhering surface sensor is an NTC thermistor assembly on pressure-sensitive tape that is loaded with ceramic powders; this design provides for high thermal conductivity producing precision temperature measurements. These are ideal for applications such as ice machines, liquid chillers, vending machines, beverage dispensers, ice cream machines, and coffee machines.

PTM פורסם ב: