Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
flatflex-slide18

One of the issues with ZIF connectors is that zero insertion force typically means zero withdrawal force. As a solution to this problem, FCI has built in a feature called ZIF with prehold into many of their connectors. This innovation provides a small amount of retention to the cable, holding it in place until the actuator provides the final locking. This prevents the cable from unintentionally slipping out and creating unnecessary rework.

PTM פורסם ב: