Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
flatflex-slide22

As connectors continue to be developed with smaller pitches and lower profiles, issues regarding board processing become more prevalent. Lower profile connectors have a much higher risk of solder wicking beyond the tails and up into the mating interface. This creates short circuits and, in some cases, renders the connector mechanically unusable. In order to address this concern, FCI employs a proprietary process which places a barrier of nickel between the solder tails and the interior of the connector. This barrier prevents solder from wicking and depositing where it can create quality problems and the need for rework.

PTM פורסם ב: