Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
flatflex-slide7

Flex circuit connectors are available in multiple contact spacing options, ranging from 1.25mm  down to 0.20mm. There are connectors for flexible circuitry with larger contact spacing (2.54mm) but they are typically two piece connector solutions. Contact spacing, also referred to as pitch, is the distance between contacts in the same row measured center to center. The contact spacing chosen usually reflects the application’s demand for printed circuit board space. For example, the designer of a handheld device places a premium on getting the maximum number of components in the smallest package.

PTM פורסם ב: