Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
RFID-Slide24
In contrast to passive RFID, active solutions typically include a power supply in the tag, which is in most cases a battery. The main difference when compared to passive solutions is the extended communication distance that can be achieved with active RFID. A potential drawback is that the battery capacity limits the lifetime of the tags. Microchip solves this issue by combining LF RFID and UHF technology within one chip, thus extending the battery lifetime to a maximum. Applications requiring large read/write distances are basically tracking-related systems such as: assets, containers, and industrial automation but also include people or animals. Since the tag incorporates an MCU, sensor signals can also be read and transmitted.
PTM פורסם ב: