Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
RFID-Slide9
This slide shows some typical tag form factors. On the upper left are shown the well-known ISO or clamshell cards, and below, several key fobs. Both are mainly used for access control systems. The image on the top shows a so-called E-unit which is typically packaged in a plastic housing and then attached to the ears of cows, sheep, goats and pigs. The upper right image shows glass transponders which are injected under the skin of the animal. E-units are also used in any kind of circular disc tags for general identification purposes. Microchip's complete tag solution, a transponder, is shown bottom right. This type of tag is commonly used in the automation industry.
PTM פורסם ב: