Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide14

Over time, charge (electrons) may leak from the memory cells through the transistor floating gate resulting in a change in logical bit state and thereby potentially causing data corruption. As shown here in the diagram, a memory cell starts its life with the ability to hold electrons well resulting in the logical state expressed as expected. Once the memory device is put into use, this ability deteriorates resulting in fewer than expected electrons “held” in the floating gate of the cell. This could potentially cause data corruption if not identified and corrected.

PTM פורסם ב: