Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide20

microSD and full size SD cards are very compact footprint NAND media devices and do not allow for the addition of capacitors to prevent issues resulting from unstable power supply. These devices implement passive protection features for risk mitigation. This is known as ATP PowerProtector Lite. Such features are enabled at a firmware level, and typically include the creation of redundant copies of firmware to serve as backups in case of corruption of the master firmware during run time. These backup firmware copies are created and stored in the NAND Flash at locations that are less susceptible to corruption. Multiple logical to physical address mapping tables are also present enabling successful roll-back/restore points.

PTM פורסם ב: