Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
AMS22U-Slide2
The Bourns® AMS22U position sensor is one of the Bourns® electromechanical sensing products based on a non-contacting magnetic sensor. The core of this rotary position sensor is a programmable quad Hall effect integrated circuit that provides a signal which is converted into a voltage output. The AMS22U position sensor is programmed at the factory to meet any rotational angle between 10 and 360°. It is particularly well-suited for harsh environments and long life applications.
PTM פורסם ב: