Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
AMS22U-Slide8
Shown on this slide are the significant features of the AMS22U. The design is based on non-contacting magnetic technology using a magnet and a programmable quad Hall effect IC. Because the sensor is non-contacting, it is compatible for use in harsh environments typically encountered in industrial applications such as vibration, shock, and fluid/dust ingress. The position sensor is programmable for various angles of rotation and the performance is highly repeatable. This product is also compliant with current RoHS directives.
PTM פורסם ב: