Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
for low light

Some 4 to 20 milliAmps displays come with annunciators that can be illuminated,°F” and°C”, “%” and “PSI”. All of these units come with customer selectable decimal points for display purposes. For applications that have low light, many of the meters come with optional backlighting. A separate 24 Volt DC power supply can be used to power the backlighting or it can be powered off the loop, as long as 24 VDC is available. If a separate power supply is used, the ground should be tied to the current loop ground.

PTM פורסם ב: