Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
physical size

When it comes to choosing meter sizes and mounting, in the C-Ton meter line, there are many options available. The physical size of the digital panel meters ranges from the smallest, an LCD of less than .4 inch digits, to the largest, an LED at 2.3 inch digits. Mounting choices are bezel mounting, window or surface mounting, and wall or ceiling mounting (BDR).

PTM פורסם ב: