Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
HE-Slide13

As a standard option, the joystick may be fitted with a mechanical limiter plate to limit the throw of the joystick to a given shape. For example, a plus shape would not allow the user to move the joystick North and East simultaneously. Alternatively a square limiter will allow full travel on both the X and Y axis at the same time in a diagonal movement. Joysticks can be supplied with many wiring options, including a variety of cable lengths, gauges and connector types.

PTM פורסם ב: