Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Digital-Slide6

The PG-100B series inherits many of the features from the PG-100N series such as Si chip for excellent stability, easy one-handed operation, large 3½ digit LCD display, long battery life, automatic power off, one-touch zero-point calibration, and analog output. On top of these features, PG-100B uses SUS316L stainless steel diaphragm for pressure sensing which allows the PG-100B series to measure both gas and liquid pressure. Pressure units can be changed in selected models.

PTM פורסם ב:
PTM Updated on: 2019-08-06