Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25
Encoders Provide Directional Information

Detection of shaft direction is very useful and even critical to some applications. For example, in a radio, the rotational direction of the volume knob tells the receiving circuit whether to increase or decrease the volume with each square wave. In automation equipment, the rotational direction is detected, and other operations are initiated when a pre-set number of pulses for that direction has been achieved. An elaborate and sophisticated set of movements can be executed automatically to perform tasks like placing components on a PC board, welding seams in an automobile body, moving the flaps of a jumbo jet, or just about anything that involves a set of precise motions. In the upper illustration here, signal A leads B; signal A outputs a rising edge before signal B. This indicates the shaft is rotating counter-clockwise. In the second illustration, signal B leads A. This indicates the shaft is rotating clockwise.

PTM פורסם ב: