Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25
Encoders Provide Speed Information

Encoders can detect speed when output pulses are counted in a specified time span. The number of pulses in one revolution must also be known. In the equation given here, S represents speed, C represents the number of pulses counted, PPR the resolution of the encoder, and t represents the time interval, in seconds, during which the pulses were counted. The second equation shows that if sixty pulses are counted in a time interval of ten seconds using a 250 CPR encoder, the shaft speed is 1.44 RPM.

PTM פורסם ב: