Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
CliQ Series DIN Rail Power Supplies Slide 17

A design characteristic of the CliQ family is the full aluminum casing which provides complete case corrosion protection in harsh corrosive operating environments. Rust particles, which can be harmful to the components inside during operation, are prevented.

PTM פורסם ב: