Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Common-Circuit-Slide10

Unlike a fuse rating, a circuit breaker rating indicates the maximum current the circuit breaker will consistently maintain at an ambient room temperature. Thus, a 10A circuit breaker will maintain a 10A current without nuisance tripping. In fact, a typical 4A circuit breaker with a slow trip profile will tolerate a temporary 10A current surge without nuisance tripping. Oftentimes, nuisance tripping is caused by in-rush currents associated with certain electrical components – primarily motors, transformers, solenoids, and large capacitors. In such cases, the designer needs to specify a circuit breaker with a delay. Thermal circuit breakers have a natural delay, and magnetic circuit breakers can have added hydraulic delays. When designing equipment with high in-rush currents, match the delay to the duration of the expected in-rush current.

PTM פורסם ב: