Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Common-Circuit-Slide29

Interrupting capacity is the maximum amperage a circuit breaker can safely interrupt. Circuit breaker Interrupting capacity is the maximum amperage a circuit breaker can safely interrupt. Circuit breaker manufacturers publish this specification along with the number of times the circuit breaker will perform this feat. For example, E-T-A publishes two types of interrupting capacity specifications. One is called Icn, or Normal Interrupting Capacity –is the highest current the circuit breaker can interrupt repeatedly. The Normal Interrupting Capacity reflects the circuit breaker quality. The other specification is UL 1077 Interrupting capacity – which is defined as the maximum current a circuit breaker can safely interrupt at least one time without causing a fire hazard.

PTM פורסם ב: