Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Common-Circuit-Slide28

Thermal circuit breakers will trip at high amerage in a cold environment, and it will trip at a lower amperage in Thermal circuit breakers will trip at higher amperage in a cold environment, and it will trip at a lower amperage in a hot environment. For example, motor windings need more protection from overheating at 90°C than the same windings at 20°C. A cold motor requires  more in-rush current to get started, and therefore a longer delay is advantageous on a cold day. Another misconception is that magnetic-hydraulic style circuit breakers are immune to performance changes in rising ambient temperatures. On the contrary, these circuit breakers contain a dashpot with a liquid core that becomes more fluid at higher temperatures – in turn reducing the time of the hydraulic delay.

PTM פורסם ב: